Technical FAQs

Ask a Question

What is the max speed of ATV320 drive at deration of motor?
The max speed of ATV320 drive at deration of motor depends upon speed range of the ATV320 drive. The speed range of ATV320 drive is 0.1 hz to 50hz...
What is the output short circuit capability and duration for ATV320 drive?
The output short circuit capability and duration for ATV320 drive is 10 *In drive during 10µs
What is the frequency accuracy of the AC output of ATV320 drive?
The frequency accuracy of the AC output of ATV320 drive is +/- 10 % of nominal slip 0.2 Tn to Tn.
What is the overall power factor for ATV320 at different load?
The overall efficency of ATV320 at different load is    Different load          Overall efficiency     100% 0.555      75%                       ...
What is the overall efficency for ATV320 at different load?
The overall efficency of ATV320 at different load is    Different load          Overall efficiency     100%                        0.984     75% ...
How much power is applied by each M580 safety I/O module to its non-safety functions.
5VDC power provided by the backplane is applied by each M580 safety I/O module to its non-safety functions. 
Is 140ACO02000 supports channel to channel isolation.
Yes, 140ACO02000 do support channel to channel isolation , below are the isolation details:   500 VAC @ 47 ... 63 Hz or 750 VDC for 1 minute
What are the Modbus TCP explicit Messaging limitations with BMENOP0300 module.
The BMENOP0300 module presents the following Modbus TCP explicit messaging feature as shown in below table:
What is the maximum number of concurrent IED client connections possible with BMENOP0300 module.
Maximum number of concurrent IED client connections possible with BMENOP0300 module is 32.
Is it possible to assign multiple 140CRA31908 as I/O master.
NO, Only one 140CRA31908 module is assigned the I/O master at any time. The master 140CRA31908 module can perform these tasks:  Manage I/O modules...
Results 71 - 80 of 100