Customer Story: Baosteel

    Steel production goes DIGITAL

    Chinese steel giant Baosteel transforms its steel manufacturing with EcoStruxure™ Plant

    Watch the video
  • Shanghai Baosteel Group Corporation (Baosteel) Smart manufacturing for the steel industry

    Chinese steel giant Baosteel transforms its steel manufacturing with EcoStruxure Plant, increasing production by up to 30%, improving worker safety, and reducing labor costs.

The Challenge

Baosteel, the largest modern steel-producing enterprise in China, decided to upgrade its 1580 smart hot rolling workshop as a pilot project for the "Made in China 2025" initiative, championed by the Ministry of Industry and Information Technology. With its digital transformation, Baosteel sought to address:

• Rising labor costs
• Tighter operational safety standards
• Energy efficiency
• Lack of innovation

Officially launched in September 2016, the workshop is set to become an automatic, unmanned, and smart platform for product manufacturing management.

baosteel-1-26-IC-980x890
Default Alternative Text

“The implementation of unmanned operation for the slab yard in the hot rolling workshop is widely considered to be the most difficult part. With Schneider Electric’s expertise in energy management and automation, the 1580 hot rolling workshop will see significant improvement in engineering control, efficient and smart operation, safety and reliability.”

Wenqing Yuan, Hot Rolling Mill Plant Director, BaoSteel 

The Solution

Productivity and Safety with EcoStruxure Plant

Apps, Analytics & Services: Expert engineering services   
Edge Control: Modicon M580 PAC, SCADA, and Partner software solution (Fluxx by Synthetis) for management of crane and warehousing operations
Connected products: Altivar Process drives, Magelis HMI, circuit breakers, inverters and switches  

Schneider Electric’s EcoStruxure Plant delivered the automation solution, technology, and services that Baosteel sought for this major project:

Industry solutions for unmanned cranes: A complete set of offers, including circuit breaker, inverter, Modicon M580 PAC, safety PAC, switch, Fluxx crane management software, and energy management system
Optimized hoisting and logistics system algorithm: Key equipment, including special sensors, ensure an optimal operational state during unattended operation
Connected systems: Operational conditions of all equipment are monitored in real time; digital operation of manufacturing equipment is empowered; and supply chain control and decision-making processes are carried out in an intelligent manner
Expert engineering services: Expert guidance and customized solutions were provided based on a wealth of industry experience and in accordance with Baosteel's specific needs. The solutions include a three-level service system for local and remote services, to ensure timely responses to the customer's requirements

The Results

With the EcoStruxure Plant solution, Baosteel has realized its goal of unmanned and automatic operation in its 1580 smart hot rolling workshop:

• 30% improvement in productivity
• Reduced labor costs: The solution has enabled 98% of crane operations to be fully autonomous which has reduced labor requirements, significantly improved work efficiency, and effectively ensured the safety of operators
• With an average daily output of up to 10,500 tons, the slab stack transfer rate has been increased from its original 30% to between 70% and 80%, greatly improving logistics management and completely eliminating material losses
• Reduced mechanical wear and more efficient asset maintenance and utilization
• Digital operation and higher level of intelligence for the complete supply chain, analysis, and decision-making process

Experience the smart manufacturing transformation with EcoStruxure Plant

Discover more
Chat with us

Do you have questions or need assistance? We’re here to help!