Building Automation & Control Systems

    Building automation begins with our innovative building management, power management systems and small building control products which enable intelligent buildings that inspire occupant productivity and deliver optimal energy and operational efficiency.

Building Automation & Control Systems

Building automation begins with our innovative building management, power management systems and small building control products which enable intelligent buildings that inspire occupant productivity and deliver optimal energy and operational efficiency.

Select Featured Products

Building Facts

  • Blue smart city icon 42% of the world's energy is used in buildings.
  • Default Alternative Text 50% of energy used in buildings is wasted because of inefficient building management systems.
  • Blue tools icon In developed economies, at least half of the buildings expected to be in use in 2050 have already been built.
  • Default Alternative Text Only 25% of building costs are associated with capital expenses, while 75% of costs are used to operate a building over its life cycle.
  • Blue EcoXpert icon Only 20% of facility managers use 80% of the available capabilities in their building management systems.
  • Default Alternative Text 30% of energy used in buildings is waste.
  • Case Studies The Edge

    Schneider Electric provides building automation to help make The Edge the world’s most sustainable office building.

  • T-Mobile Arena – The Show Must Go On Creating an awe-inspiring event complex with EcoStruxure
  • EcoStruxure™ Power - How IoT-Enablement is Taking Power Distribution to New Limits See how digitizing power distribution is taking building safety, reliability, and efficiency to new limits.
Chat with us

Do you have questions or need assistance? We’re here to help!