Open Compute Solutions

    Deploying open IT hardware solutions into a new or existing facility? Schneider Electric has done the research and developed the solutions enabling you to do things right.

    + Lifecycle Services

Is your data centre ready for Open Compute Solutions?

Rack scale architectures and open hardware solutions are challenging the status quo for computing deployments. As an Open Compute Project (OCP) Platinum Member and a member of the Open19 Foundation, we are participating in the development of new solutions and have done extensive research to understand the impact and benefits of these new technologies.
  • We are an OCP Platinum Member

    Started in 2011 by Facebook, Intel, Rackspace and Goldman Sachs, The Open Compute Project (OCP) is a collaborative community focused on redesigning hardware technology to efficiently support the growing demands on compute infrastructure. As a Platinum Member of OCP, Schneider Electric is taking a leadership role in shaping tomorrow's data centres.

    Learn more
    Default Alternative Text
  • Default Alternative Text
    HyperPod The backbone of your data centre, HyperPod provides integrated cabling infrastructure, containment and branch circuit distribution for rapid deployment of fully integrated racks. Find out more
  • Scorpio PSU
    Rack Power Supply Unit (PSU) Power supplies consolidated at the rack level offer benefits in cost and efficiency. Schneider Electric offers several 12VDC configurations to meet a variety of density and redundancy needs.
  • Default Alternative Text
    Rack Battery Backup Unit (BBU) Working together with a 12VDC rack PSU, this scalable shelf can provide up to 15 kW of redundant power for 120 seconds. To find out more, contact us with the form at the bottom of this page.
  • Default Alternative Text
    Open Rack Compatible with the OCP V2 specification, this rack allows for the installation of OCP ITE. To find out more, use the contact form at the bottom of the page.
  • An OCP Inspired™ solution

    Compatible with Open Compute V2 rack specification, this 2OU, 12VDC rack PSU has earned OCP Inspired™ recognition. Major features include:

    • 15 kW N+1 or 9 kW 2N configurations
    • Input ATS for dual feed
    • Can monitor up to 2 BBU shelves
    • Software defined power compatible
    For more information or to order, use the form at the bottom of this page.

    OCP Inspired PSU Gemini
  • Data Centre IT Pod Specs

    Optimising POD design creates an architecture that's scalable and repeatable, simplifies power and cooling infrastructure, facilitates roll-in and out OCP racks and maximises white space.

Custom Capabilities

Today's IT solutions are evolving quickly. Our team of R&D experts can work with your hardware and software development team to create rack scale solutions to meet your business needs. Consider our team and supply chain as an extension of your business.