India
Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website for company information.

Select your location
  • Default Alternative Text

    Single Drive booster

    Solution with the best functionality/cost ratio for simple machines, up to 1 circuit for 2 compressors

Default Alternative Text

Solution

With the all-in-one Magelis SCU, the architecture is a cost-efficient solution.

Simple, standard boosters are the first step toward automation, moving away from traditional relay architectures. Single-drive boosters can be used in single- or multi-drive mods.

Benefits

> Capable of managing multiple pumps using one drive
> Maintains constant pressure in the system with PID, pump stage and de-stage-related functions

> Diagnostic features for easy maintenance
> Embedded booster and pumps protection
> Operates smaller (auxiliary) pumps to maintain lower flow requirement
Chat with us

Do you have questions or need assistance? We’re here to help!